The Compact Mode offers an alternate view for the Digital Meter and Analog Meter views only. This view gives a small, simplified view of one measurement at a time and is suitable for viewing on small computer monitors.
located in the upper right corner of the Power Meter application window.
on the tools palette on the right side of the current view to switch to the Compact Mode (see example below).
from the Compact Mode display.